Compact Flash Cards

Compact flash cards, often referred to as CF cards or CFast cards, are a widely used type of memory card. Introduced in 1994, these high-performance, high-reliability memory cards are used in portable electronic devices like digital cameras, digital SLR cameras, phones and video recorders.

Compact flash cards are invaluable to photographers and professionals, especially when integrated memory is insufficient. It is important to verify which type of CF card you need, as they come in two types: Type I and Type II. Type II offers higher storage but is also a thicker card.

How Compact Flash Cards Work?

At its core, a compact flash card uses flash memory to store data through floating gate transistors. These transistors trap electrical charges, representing binary data. A built-in CF controller manages all data read and write operations, using a standard interface to ensure high performance and data integrity. This controller handles error correction and wear levelling, which prolongs the card's life and protects your data.

Features and Benefits of Compact Flash Cards

Compact flash cards offer several key features and benefits that make them a preferred choice for professionals and industrial applications:

  • Durability and Reliability: CF cards are known for their construction, making them resistant to shock, vibration, and extreme temperatures. This durability ensures high reliability and data integrity in demanding environments.
  • High-Speed Performance: With advanced technology like UDMA (Ultra Direct Memory Access) ratings, CF cards offer high-speed read and write capabilities. This high-speed performance is crucial for continuous shooting in digital cameras and recording high-definition video.
  • Wide Compatibility: Despite the introduction of newer memory card formats, compact flash cards remain widely compatible with many professional cameras and industrial devices. Their long-standing presence in the market has made them a trusted standard.
  • Versatile Applications: From professional photography to industrial data logging, the versatility of CF cards is a major benefit. They provide a high-performance, reliable memory solution for devices that require removable and robust data storage.

Applications of Compact Flash Cards

Compact flash cards are used in a variety of industries where reliable and high-speed data storage is essential.

Professional Photography and Videography

In professional photography and videography, CF cards are a standard for their high-speed performance and reliability. They handle large files generated by high-resolution cameras, ensuring photographers and videographers can capture every moment without delay.

Industrial Automation and Control Systems

Industrial compact flash cards are a reliable solution for industrial automation and control systems. They are used in programmable logic controllers (PLCs), human-machine interfaces (HMIs), and other industrial devices for storing configuration files, programme data, and operational logs.

Data Logging

In data logging applications, industrial CF cards are used to reliably record data from various sensors and instruments over long periods. Their durability and high memory integrity make them an ideal choice for collecting critical data in challenging environments.

Embedded Systems

Compact flash cards are used in embedded systems, such as single-board computers, where a compact and reliable form of non-volatile memory is required. Their robust design makes them suitable for use in embedded systems in aerospace, automotive, and other demanding industries.

Types of Compact Flash Cards

Compact flash cards are categorised by physical type, capacity, application, and speed to meet diverse needs.

  • By Physical Type: CF cards come in two physical types: Type I and Type II. Type I is the more common, thinner format. Type II is slightly thicker and can accommodate higher-capacity memory cards. CFast cards are a newer standard with a different interface, offering even faster speeds.
  • By Capacity: CF cards are available in a range of capacities, from a small 2GB compact flash card to much larger capacities like 16GB and 128GB, catering to different storage requirements.
  • By Application: You can choose between consumer-grade and industrial CF cards. Industrial compact flash cards are built with higher-quality components to withstand extreme temperatures, vibration, and shock, ensuring greater reliability.
  • By Speed: The speed of a CF card is determined by its UDMA (Ultra Direct Memory Access) rating and its write speed in MB/s. Higher UDMA ratings and faster write speeds are crucial for high-resolution photography and videography.

How to Install Compact Flash Cards

Installing a compact flash card is a straightforward process, but proper handling is key to preventing damage and ensuring data integrity.

  1. Prepare the Device: Ensure the device, whether a camera or an industrial controller, is turned off before you begin. This prevents data corruption and damage to the card or the device.
  2. Locate the Card Slot: Find the memory card slot, usually located on the side of the device or in the battery compartment.
  3. Orient the Card Correctly: Insert the compact flash card into the slot, making sure it is oriented correctly. The card should slide in smoothly without force. Never force a card into the slot, as this can damage both the card and the device.
  4. Secure the Card: Gently push the card into the slot until it clicks into place. Some devices may have a latch or lever to secure the card.

How to Choose the Right Compact Flash Cards

Selecting the right compact flash card is crucial for ensuring compatibility, performance, and reliability. Here are several factors to consider:

  • Device Compatibility: Always check the manufacturer's specifications to ensure the CF card is compatible with your device. Some devices may only support specific card types, capacities, or speeds.
  • Capacity: The capacity of the CF card you choose depends on your storage needs. For example, a 4GB CF card may be sufficient for a few hundred photos, while a larger capacity card is better for extended video recording or data logging.
  • Speed: The speed of the CF card is crucial for performance. For high-resolution photography or videography, choose a card with a high UDMA rating to ensure fast write speeds and seamless data capture.
  • Durability: For industrial or rugged applications, choose an industrial compact flash card for enhanced durability and reliability. These cards are designed to withstand harsh environments and provide long-lasting performance.

Compact Flash Cards Manufacturer, Supplier & Distributor in Australia

RS Australia is your trusted manufacturer, supplier, and distributor of high-quality compact flash cards. Our extensive selection provides exceptional value, with competitive pricing that fulfils all your requirements. From a basic 1GB compact flash card to a high-capacity 2TB flash card, we offer reliable components from leading brands like InnoDisk, Transcend, and ATP, ensuring peak performance for every project.

To provide a complete solution for your requirements, we also carry other computing equipment and computer peripherals, such as SD cards and network hubs. Order online today for fast delivery across Australia.

For more information on our delivery options and fees, please refer to our Delivery Page.

70 Products showing for Compact Flash Cards

Results per page

Be the first to know about our latest products and offers

Email address

The personal information you provide to us when signing up to this mailing list will be processed in line with the Privacy Policy